Skip to Content


Skip over secondary navigation

Secondary navigation

Content

Wednesday, February 18, 2009

New Bus Link Reduces Costs to Modernize Siemens APACS+ Process Control Systems

ATLANTA — Modernizing APACS+ installations to the SIMATIC® PCS 7 process control system is now more cost effective than ever with the APACS+ DP IOBUS Link from Siemens Energy & Automation, Inc.

The APACS+ DP IOBUS Link allows plants to upgrade their existing APACS+ controllers, while retaining the existing APACS+ I/O Modules and field wiring terminations.

Additionally, using the DP IOBUS Link delivers more computing power to existing systems -- including the ability to select multiple scan rates as fast as 10 milliseconds.  This modernization will help extend the life and lower the total cost of ownership of the APACS+ system. It also retains existing field wiring and I/O for significant cost savings.

“Siemens continues to sell and support APACS+,” said Ken Keiser, Siemens process automation marketing manager. “The new bus link is a good example of how the company is investing in APACS+ and helping customers get the highest possible return on their investment.”

For more about APACS+ DP IOBUS Link log on to www.sea.siemens.com/migration or call 800-964-4114.

 
 

Contact Information:

For Media Inquiries:

Michael Krampe
Press and Analyst Relations
Call: 770-751-2211  
3333 Old Milton Parkway
GA 30005 Alpharetta,

michael.krampe@siemens.com