| |
Measuring Level in Flotation Cells
|
The Probe monitor uses non-contacting ultrasonic technology to provide
reliable measurement of froth levels in the flotation cell. |
Phelps Dodge Mining Company, the mining and metals division of Phelps
Dodge Corporation, is one of the world's leading producers of copper and
molybdenum and is the world's largest producer of continuous-cast copper
rod. The Bagdad copper mine, located in Arizona's Yavapi County, produces
copper and molybdenum ore, and has a history that dates back to the late
19th century.
The facility uses a large series of cone crushers and ball mills to reduce
copper ore to very fine particles. Then the solids are "pulped" or mixed
with water to create a slurry. To this slurry, they add milk of lime to
raise the pH. Small amounts of special reagents are also added, including
a frother to make bubbles, as well as a collector chemical that causes the
copper minerals to stick to those bubbles. This material is pumped to a
series of froth flotation cells to concentrate the copper. Air is blown
into the flotation cell tank, and the pulp mixture is vigorously agitated
like a high-speed blender. Rising bubbles carry the copper particles up
and over the edge of the flotation tank. The bubbles break soon after they
flow over the edge. The copper is then ground even finer and purified by
additional flotation processes.
|
|
It
is critical to measure the level of both the pulp and the froth to ensure
optimum copper concentrate production. Those levels provide feedback to
the plant's process control system so operators can make appropriate
changes to variables like pulp and air flow as well as the addition of
chemical reagents. It's a very difficult level measurement because of
material build-up and plugging that occurs on most types of level
technologies. In addition, the harsh conditions necessitate the
installation of a very robust device.
In
this application, Phelps Dodge uses the Probe ultrasonic level monitor
from Siemens-Milltronics. This instrument combines sensor and electronics
in a single package for effective liquid level measurement in open or
closed vessels. It is easy to install and remove, and the non-contacting
ultrasonic technology requires virtually no maintenance. The instrument
does not touch the slurry. The Probe monitor features patented Sonic
Intelligence®
echo-processing that filters out false echoes from acoustical or
electrical noises and agitator blades in motion, giving superior
measurement reliability.
Each flotation cell is equipped with a Probe to monitor the froth level. A
second Probe measures the pulp level based on a metal target attached to a
mechanical float assembly. The 4 — 20 mA analog output from the Probe is
fed into the plant's control system to provide flotation cell level
information.
The
requirements for measurement are relatively narrow. The span for the pulp
measurement (using the Probe with target and float assembly) is 10 inches
and the froth level Probe uses a span of only two inches.
The Probes are very easy to program and they require no maintenance. The
only set-up required is programming the span for the analog output. This
is easily accomplished in the instrument shop or during installation. The
Probes are proving to be a much better alternative to older bubbler
technology. The company has Probes successfully installed at other
properties as well.
more
product info 
|
Note:
Please
forward all leads/inquiries to:
Siemens Energy & Automation, Inc.
Process
Solutions Division, Mail Stop 510
PO Box 900,
1201
Sumneytown Pike
Spring
House, PA 19477-0900
Or
call (215) 646-7400
To receive future
news updates by e-mail, subscribe to PINEWS at
http://www.sea.siemens.com/ia/newsprod/inpinews.html
CONTACT:
Teresa
Parris
Marketing Communications Manager
(215) 646-7400 ext. 2592
Top
of Page 
|
|