Accuracy and durability of equipment have plagued the weighing operation over the years. The problem was not solved until about one year ago when the mine removed its third system and replaced it with the SIWAREX M weighing system. Some of the earlier scale systems started having problems within the first month of operation. These problems ranged from inaccurate readings and lost calibration accuracy to total failure.
The load cells are hermetically sealed in casings of stainless steel that are impervious to outside elements-even for the harshest conditions. As coal ore is deposited inside the weigh cell, a compensation arm inside the load cell triggers a phototransistor switch, activating an electromagnetic coil. This causes a corresponding voltage change across a connected load resistor. The change is sent to a processing module that interfaces with a programmable controller.
Configuration software provided by Siemens runs on standard PC platforms. Working with the data provided by the weigh scale module, the software provides for easy setup of such functions as tare (container weight compensation), gross weight, net weight, scale standstill messages, calibration, automatic zero offset, coarse/fine feed signals, limit value generation, tolerance monitoring and filter parameters. The weigh scale modules allow calibration to be controlled with 20-bit sampling that provides an accuracy of 0.05 percent with 65,000 division resolution, ± 524,000 parts. The system has an EU rating of Class III, 6000d.
All the parameters are configured and stored in the Siemens SIMATIC(r)505 programmable logic controller (PLC). The weigh scale modules snap on a standard DIN rail inside the control cabinet just below the PLC. There are two modules, one for each load cell. The modules can be replaced in just a few minutes. This requires no re-calibration of the scales because the parameters are downloaded from memory.
The modules come standard with an RS232 port for connecting to a printer, PC or host. They also have a 20 mA connector for interfacing a third-party human machine interface that the control room uses to report the activity being transmitted from the trip stations and the weigh areas.
There are also status LEDs on the modules that indicate system errors, operation errors, calibration mode, scales standstill, 0.25e zero and scales adjusted status. Additional LEDs show the 24V power supply operation, the data activity of the three digital inputs and four digital outputs, as well as the analog output and the load cell connection status.
The control room on the surface for the hoist exchanges information with the control room at the weigh stations over Ethernet. In this manner, the technician at the bottom of the shaft and the technician at the surface level know what is happening in either area. Alarms and interlocks built-into the respective PLC system programming provide virtually trouble free automated operation.
 | Information from the two SIWAREX weigh scale modules is processed through a PLC. Data provided by the weigh scale module includes tare (container weight compensation), gross weight, net weight, scale standstill messages, calibration, automatic zero offset, coarse/fine feed signals, limit value generation, tolerance monitoring, and filter parameters. As a load setpoint is reached, the PLC signals the feeder to stop, the gate for input into the weigh cell is closed, and then a signal is sent to the weigh cell to open a door, dumping the weigh cell load into the trip unit. |