General interest press release
Siemens Unveils First UL Listed Solar Safety Switch for Three 600Vdc Circuits
ATLANTA, Thursday, June 17, 2010
Siemens Industry, Inc. introduces the first heavy duty, UL listed, three-pole solar disconnect switch able to control three separate 600VDC circuits. Available in 30, 60 and 100-amp ratings, the Solar Photovoltaic Type VBII Safety Switch lowers equipment and installation costs by doing the work of three traditional switches in similar solar applications.
Unique in design, the new switch outperforms conventional safety switches by utilizing powerful magnets which are strategically located within the line bases to quickly disperse and extinguish arcs when negative-ground 600VDC circuits are opened under load. Available in fusible and non-fusible versions, the Solar Photovoltaic Type VBII Safety Switch comes in Type 1 and 3R enclosures for indoor and outdoor installations. A factory installed ground bar is standard, as is a rolled front flange that prevents damage to conductor insulation and injuries to installer’s hands.
A metal handle with a large plastic grip offers positive stop in both ON and OFF positions. Two and three-point mounting provisions are also standard as are large top, bottom and side gutters to help facilitate wiring.
For more information about the Solar Photovoltaic Type VBII Safety Switch call 800-964-4114 or log on to www.usa.siemens.com/switches.
About Siemens
Siemens Industry, Inc. (SII) is the U.S. affiliate of Siemens’ global Industry Sector business—the world’s leading supplier of production, transportation and building technology solutions. The company’s integrated hardware and software technologies enable comprehensive industry-specific solutions for industrial and infrastructure providers to increase their productivity, sustainability and profitability. The Industry Sector includes six divisions: Building Technologies, Industry Automation, Industry Solutions, Mobility, Drive Technologies and OSRAM SYLVANIA. With nearly 222,000 Siemens Industry Sector employees worldwide, the Industry Sector posted a worldwide profit of $2.7 billion on revenues of $47.7 billion in fiscal 2009. www.usa.siemens.com/Industry
A division of Siemens Industry, Inc. (SII), Building Technologies (BT) Division is a leading provider of energy and environmental solutions, building controls, electrical distribution equipment, fire safety and security systems solutions. BT’s solutions enable America’s buildings to be more comfortable, secure and environmentally friendly as well as less costly to operate. With a U.S. headquarters in Buffalo Grove, Ill., BT employs 7,400 people and provides a full range of services and solutions from more than 100 locations coast-to-coast. Worldwide, the company has 28,000 employees and operates from more than 500 locations in 51 countries. The Building Technologies Division posted worldwide revenues of $8.1 billion in fiscal 2009. www.usa.siemens.com/buildingtechnologies