Skip to Content


Skip over secondary navigation

Secondary navigation

Content

Thursday, February 12, 2009

Combined Vortex Flowmeter For Steam, Gas And Liquids

ATLANTA — Siemens Energy & Automation, Inc. today announced the U.S. introduction of the new Sitrans FX300 vortex flowmeter series, which is equipped with a temperature sensor and an optional pressure sensor.  Through the combination of these sensors into one unit, the vortex principle is used to measure the temperature, pressure and flow of steam, gases and liquids.

The new “All-in-one Solution” series is suitable for a wide range of applications in the chemical, pharmaceutical, food and beverage, oil and gas, energy generation and district heating industries. With the addition of the Sitrans FX flowmeters, Siemens now offers technologies for all flow applications in process automation. 

The new Sitrans FX300 two-wire flowmeter with Hart communication is designed for applications requiring reliable flow measurement independent of dynamic pressure, temperature, viscosity and density variations. These applications include the measurement of steam and saturated steam, monitoring of steam boilers, control of compressor outputs, consumption measurement in compressed air systems, measurement of industrial gases, burner consumption measurement, and SIP and CIP processes in the food and beverage industry and pharmaceutical industry.

 The new flowmeters are characterized by high accuracy and reliability. For example, the sensor is fully welded and does not require wear-prone internal gaskets. The operating temperature range is from minus 40 to plus 464 degrees Fahrenheit. In the case of steam and gas with flow rates of 2 to 80 meters/second, the accuracy is 1.0 percent, and in the case of liquids flowing at rates between 0.4 and 10 meters/second, it is 0.75 percent. The nominal internal diameter range is DN15 to DN300 (0.5" to 12").

 The Sitrans FX vortex flowmeter works on the vortex measuring principle. This involves detecting the frequency at which alternating vortices are shed from a buff body hit by the flowing medium. These vortices create a force on a sensor wing that moves in proportion to the volume of flow. This sensor has a dual piezoelectric crystal mounted in the wing that detects the oscillations precisely and transmits this information to the FX electronics for conversion to the actual flow rate in the pipeline.

 
 

Contact Information:

For Media Inquiries:

Michael Krampe
Press and Analyst Relations
Call: 770-751-2211  
3333 Old Milton Parkway
GA 30005 Alpharetta,

michael.krampe@siemens.com