Skip to Content


Skip over secondary navigation

Secondary navigation

Content

Monday, March 26, 2007

New SINUMERIK HT 8 Handheld Terminal At WESTEC 2007

ATLANTA -- The new SINUMERIK HT 8 Handheld Terminal from Siemens Energy and Automation, Inc. integrates an operator panel and a machine control panel into one compact device that enables the user to visualize machine applications running on multiple SINUMERIK NCU/PCU operations without reconfiguration.  The handheld unit automatically reads the configuration from the HMI main panel of the machine to which it is connected.  The HT 8 is compatible with all SINUMERIK operating panels.