Thursday, February 12, 2009
Siemens Introduces ESP200 Overload Relays
ATLANTA — Siemens Energy & Automation, Inc. has introduced the new line of self-powered ESP200TM Overload Relays for industrial and construction applications that replaces the ESP100 Overload Relay. Building on the success of Siemens NEMA starters with overload protection found in millions of motors, the new overload relay line is designed to reliably operate in the most demanding environments.
Easily configured without software or manuals, the new ESP200 line delivers unmatched repeat accuracy of 99 percent. Versatile by design, the ESP200 takes the guess work out of meeting numerous overload protection requirements. Field selectable Trip Class 5, 10, 20 or 30 can easily be set by two DIP-switches and the FLA dial allows for a wide adjustment range (4:1). This simple and versatile configuration enables companies to reduce overload relay inventories by up to 40 percent.
Ideal for oil pumping, agriculture and other applications where continuous motor operation is essential, the ESP200 line is available with automatic and remote reset features.
The easy to use relays are DIN rail mounted and feature removable terminals for fast change out without removing control wiring. Additionally, a visible trip indicator quickly allows operators to identify overloads.
Touch-safe terminals help prevent accidental exposure to live circuits. UL listed and CSA certified
according to the strictest standards, the ESP200 line offers ground fault protection that trips at 60 percent of motor current, thereby protecting motors from high resistance short circuits or ground faults due to moisture, condensation or insulation damage.
About Siemens
Siemens Energy & Automation, Inc. is one of Siemens’ operating companies in the U.S. Headquartered in the Atlanta suburb of Alpharetta, Ga., Siemens Energy & Automation, Inc. manufactures and markets one of the world’s broadest ranges of electrical and electronic products, systems and services to industrial and construction market customers. Its technologies range from circuit protection and energy management systems to process control, industrial software and totally integrated automation solutions. The company also has expertise in systems integration, technical services and turnkey industrial systems. For more information:
www.sea.siemens.com.
Siemens AG (NYSE: SI) is a global powerhouse in electronics and electrical engineering, and operates in the industry, energy and healthcare sectors. For more than 160 years, Siemens has built a reputation for leading-edge innovation and the quality of its products, services and solutions. With nearly 400,000 employees in 190 countries, Siemens reported worldwide sales of $96.6 billion in fiscal 2007. With its U.S. corporate headquarters in New York City, Siemens in the USA reported sales of $19.8 billion and employs approximately 70,000 people throughout all 50 states and Puerto Rico. For more information on Siemens in the United States, visit: