SPRING HOUSE (Oct 25, 2005) ― The Process Instruments business of Siemens Energy & Automation introduces a new generation of pressure transmitters designed specifically for the food and beverage, and pharmaceutical industries. The new Sitrans P300 pressure transmitter with stainless steel housing and measuring cell that is flush with the front panel is easy to clean and sterilize. The transmitter is suitable for process temperatures up to 392°F (200°C), and is available with the full range of sanitary connections in accordance with FDA, 3-A, and EHEDG recommendations. Common industrial process connections such as ½” NPT and ASME flanges are also available. The Sitrans P300 transmitter provides accurate and stable measurements with best-in-class performance of 0.075 percent accuracy and long-term drift of only 0.25 percent over five years.
The Sitrans P300 instrument can be easily installed locally using three keys and a display. Comprehensive diagnostics and simulation functions permit quick and simple startup of measuring circuits to help avoid plant downtime. The pressure transmitter parameters can be set using Simatic PDM software and an integral Hart or Profibus-PA interface.
Siemens Energy & Automation Inc. is one of Siemens’ operating companies in the U.S. Headquartered in the Atlanta suburb of Alpharetta, Ga., Siemens Energy & Automation manufactures and markets one of the world’s broadest ranges of electrical and electronic products, systems and services to industrial and construction market customers. Its technologies range from circuit protection and energy management systems to process control, industrial software and totally integrated automation solutions. The company also has expertise in systems integration, technical services and turnkey industrial systems. For more information: www.sea.siemens.com.
Siemens AG (NYSE:SI) is one of the largest global electronics and engineering companies with reported worldwide sales of $91.5 billion in fiscal 2004. Founded more than 150 years ago, the company is a leader in the areas of Medical, Power, Automation and Control, Transportation, Information and Communications, Lighting, Building Technologies, Water Technologies and Services and Home Appliances. With its U.S. corporate headquarters in New York City, Siemens in the USA has sales of $16.6 billion and employs 70,000 people throughout all 50 states and Puerto Rico. Eleven of Siemens' worldwide businesses are based in the United States. With its global headquarters in Munich, Siemens AG and its subsidiaries employ 430,000 people in 192 countries.For more information on Siemens in the United States: www.usa.siemens.com.
Download this article
Note: Please forward all leads/inquiries to:
Siemens Energy & Automation, Inc.
Process Instrumentation, Mail Stop 510
PO Box 900
1201 Sumneytown Pike
Spring House, PA 19477-0900
Or call (215) 646-7400
To receive future news updates by e-mail, subscribe to PINEWS