SPRING HOUSE (August, 2005) ― Siemens Energy & Automation, Inc. introduces the Sitrans LPS200 paddle switch and Sitrans LVS200 vibrating level switch, now available in high-temperature, high-pressure, and interface versions. The new products provide reliable high- and low-level alarms for a wide variety of bulk solid applications. The new high-temperature version of the Sitrans LPS200 rotating paddle switch withstands temperatures of up to 428°F (220°C). The latest high-pressure version performs in environments with pressures up to 145 psi, and the new interface version of the Sitrans LVS200 vibrating point level switch detects solids in liquids. These switches are rugged in design, are easy to calibrate, and connect to alarm and control systems.
The Sitrans LPS200 rotating paddle switch is suitable for detecting full, empty, or demand conditions in materials including grain, animal feed, cement, plastic granules, and wood chips. This latest device has a dual bearing seal for protection against dust and humidity. A friction clutch mechanism also offers protection against falling material and prevents gear failure. The standard measuring vane is suitable for materials with densities as low as 6.25 lb/ft 3, and the hinged vane can take measurements from 2.19 lb/ft 3. The paddle sensitivity can be adjusted to suit varying material properties. Configurations available include a compact version, a version with protective pipe, and one with a cable extension up to 32 ft.
The new Sitrans LVS200 vibration level switch can be installed vertically or horizontally and monitors the levels of bulk solids from a density of 1.3 lb/ft 3. The new interface version now detects solids in liquids. A pipe extension kit of up to 14 ft has also been added to the product line, allowing the electronics to be separated from the process. Fork oscillation supports self-cleaning of the device. The patented design of the fork-and-crystal assembly eliminates false high-level readings.
More information can be found on the Internet at: http://www.siemens.com/level
Siemens Energy & Automation Inc. is one of Siemens’ operating companies in the U.S. Headquartered in the Atlanta suburb of Alpharetta, Ga., Siemens Energy & Automation manufactures and markets one of the world’s broadest ranges of electrical and electronic products, systems and services to industrial and construction market customers. Its technologies range from circuit protection and energy management systems to process control, industrial software and totally integrated automation solutions. The company also has expertise in systems integration, technical services and turnkey industrial systems. For more information: www.sea.siemens.com.
Siemens AG (NYSE:SI) is one of the largest global electronics and engineering companies with reported worldwide sales of $91.5 billion in fiscal 2004. Founded more than 150 years ago, the company is a leader in the areas of Medical, Power, Automation and Control, Transportation, Information and Communications, Lighting, Building Technologies, Water Technologies and Services and Home Appliances. With its U.S. corporate headquarters in New York City, Siemens in the USA has sales of $16.6 billion and employs 70,000 people throughout all 50 states and Puerto Rico. Eleven of Siemens' worldwide businesses are based in the United States. With its global headquarters in Munich, Siemens AG and its subsidiaries employ 430,000 people in 192 countries.For more information on Siemens in the United States: www.usa.siemens.com.
Note: Please forward all leads/inquiries to:
Siemens Energy & Automation, Inc.
Process Instrumentation, Mail Stop 510
PO Box 900
1201 Sumneytown Pike
Spring House, PA 19477-0900
Or call (215) 646-7400