Skip to Content


Skip over secondary navigation

Secondary navigation

Content

FOR IMMEDIATE RELEASE

LR 200

SIEMENS Radar Level Transmitter gains approval for hazardous area installations

SPRING HOUSE (August, 2005) ―    Siemens Energy & Automation, Inc. announces that Siemens  has received the CSA, FM, and Atex approvals for its Sitrans LR 200 radar level transmitter. This allows the device to be used in hazardous areas containing flammable gases, such as in the chemical and petrochemical industries, without the requirement for an intrinsically-safe barrier.

The Sitrans LR 200 instrument is a 2-wire, loop-powered pulse radar transmitter for level measurement of liquids in bulk storage or process vessels. The device is suitable for the chemical, pharmaceuticals and petrochemical industries. Typical applications are liquids with high temperatures, high pressure, vapor or vacuum. The device is easy to install, program and operate using the four-language, alphanumeric display and the intrinsically-safe, infrared, handheld programming device. The housing lid need not be opened, even in the Ex area.

The instrument is easy to set up. Two parameters are sufficient for the basic function, and there is no need for echo profile analysis at startup. The compact electronics are mounted on a rotating housing. This can be adjusted to facilitate connection and guarantee a good view of the measured value display after installation.  The Sitrans LR 200 level transmitter offers high immunity to condensation or other deposits, works at the low frequency of 6.3 GHz and supplies signals for measuring ranges up to 65 feet. The patented Sonic Intelligence Software for signal processing is extremely reliable. In addition, Auto False-Echo Suppression detects and suppresses false echoes from tank obstructions.

More information can be found on the Internet at: https://pia.khe.siemens.com/index.asp?Nr=7427

Siemens Energy & Automation Inc. is one of Siemens’ operating companies in the U.S. Headquartered in the Atlanta suburb of Alpharetta, Ga., Siemens Energy & Automation manufactures and markets one of the world’s broadest ranges of electrical and electronic products, systems and services to industrial and construction market customers.  Its technologies range from circuit protection and energy management systems to process control, industrial software and totally integrated automation solutions.  The company also has expertise in systems integration, technical services and turnkey industrial systems.For more information:  www.sea.siemens.com.

Siemens AG (NYSE:SI) is one of the largest global electronics and engineering companies with reported worldwide sales of $91.5 billion in fiscal 2004. Founded more than 150 years ago, the company is a leader in the areas of Medical, Power, Automation and Control, Transportation, Information and Communications, Lighting, Building Technologies, Water Technologies and Services and Home Appliances. With its U.S. corporate headquarters in New York City, Siemens in the USA has sales of $16.6 billion and employs 70,000 people throughout all 50 states and Puerto Rico. Eleven of Siemens' worldwide businesses are based in the United States. With its global headquarters in Munich, Siemens AG and its subsidiaries employ 430,000 people in 192 countries. For more information on Siemens in the United States: www.usa.siemens.com. 

Note:    Please forward all leads/inquiries to:
              Siemens Energy & Automation, Inc.
              Process Instrumentation, Mail Stop 510
              PO Box 900
             1201 Sumneytown Pike
             Spring House, PA  19477-0900

             Or call (215) 646-7400

 
 

08/01/2005


Product Information

Capacitance Level
P300 Pressure Transmitters
Mag 8000 electromagnetic flowmeter