Skip to Content


Content

Tuesday, June 03, 2008

New Slider-Bed Belt Scale For Light-To Medium-Duty Loads

ATLANTA -- Siemens Energy & Automation, Inc. today announced the introduction of a new slider-bed belt scale that measures light-to-medium-duty loads. The Milltronics Weighdeck 600, with IP67 degree of protection, is suitable for flat belt conveyors transporting dry products as well for Intralox style belts conveying wet products. As a system, including an integrator and a speed sensor, daily production totals can be tallied. The areas of application range from food and beverages through pharmaceuticals to the tobacco industry.

 
 

Contact Information:

For Media Inquiries:

Michael Krampe
Press and Analyst Relations
Call: 770-751-2211  
3333 Old Milton Parkway
Alpharetta, GA 30005

michael.krampe@siemens.com