Skip to Content


Skip over secondary navigation

Secondary navigation

Content

Wednesday, March 18, 2009

Siemens PCS 7 Enhancements Reduce Engineering and Lifecycle Costs

ATLANTA — Siemens Energy & Automation, Inc. has enhanced its Simatic® PCS 7 Process Automation System with new features designed to reduce engineering and lifecycle costs.Advanced Process Library

Version 7.1 of Simatic PCS 7 includes a new “Advanced Process Library” that offers pre-engineered function blocks, faceplates and human machine interface symbols. Unlike typical library offerings that are relatively basic, the PCS 7 version 7.1 Advanced Process Library offers comprehensive functionality, greatly reducing the need for costly engineering customization and improving long term supportability.

Additionally, the Advanced Process Library’s faceplates have been designed to be more ergonomic and intuitive for the operator by linking them to other displays containing related process information.  For example, the motor faceplate contains links that will allow the operator to easily trace the cause of the first out interlock and correct the condition. The standard PID controller faceplate contains a link that automatically calls up an integrated control performance monitoring display making it easy to analyze the control performance of the loop to identify valves that require maintenance or impact product quality. 

“Siemens worked extensively with our alliance customers during the product definition process to ensure that the library met their specific requirements and those of the overall market,” said Todd Stauffer, Siemens PCS 7 marketing manager.  “The new library will help these customers meet their automation requirements today and in the future.”

Online Recipe Changes

PCS 7 version 7.1 also includes improvements that support reduced time to market and production optimization by providing a new level of flexibility for batch processes. Control recipes can be modified while running thereby giving operators greater flexibility to address unplanned events or to fine tune a recipe. As-run recipes can be saved as a new Master Recipe for future usage.

 Better Trending and Reporting

The new version offers enhancements in historical / real-time trending and reporting. Operators and engineers can analyze production data and alarms working with Excel to better monitor, track and document key performance indicators.

As with previous versions of the PCS 7 system, version 7.1 breaks traditional DCS limitations by offering the world’s only platform that integrates new and existing automation systems (process, batch, discrete and safety) and devices (instrumentation, analytics, motors, drives and safety instrumented functions) within a single platform. The system also boasts common tools for engineering, visualization and plant-wide asset and maintenance management.

For more information about Siemens Simatic PCS 7 version 7.1, call (800) 964-4114 or log on to www.sea.siemens.com/process

 
 

Contact Information:

For Media Inquiries:

Michael Krampe
Press and Analyst Relations
Call: 770-751-2211  
3333 Old Milton Parkway
GA 30005 Alpharetta,

michael.krampe@siemens.com