Skip to Content


Content

NEW! Intelli-Arc Diagnostic Tool

Easily troubleshoot any AFCI circuit!

Siemens is proud to announce the launch of the Intelli-Arc Diagnostic Tool.  The new diagnostic device makes it easier to troubleshoot AFCI circuits by improving troubleshooting accuracy and reducing the number of visits to the problem site. The diagnostic tool can be used with any circuit breaker, regardless of brand.

Arc faults are often intermittent which can make troubleshooting the branch circuit very difficult. In these cases, it is important to determine whether the fault condition exists in the permanent wiring, in connected equipment, or in a power cord.

The Siemens Intelli-Arc Diagnostic Tool helps to accurately diagnose the circuit in which a fault has occurred. When used in conjunction with good troubleshooting techniques, this tool allows the electrical contractor to determine and locate the root cause or source of the fault. The device presents information as to the type and magnitude of fault. Since the fault may not cause an AFCI to trip for various reasons, i.e. duration too short, current level too low, the tool provides an indication showing how close an event is to causing an AFCI to trip.

Click here for Technical Specifications 

 
 

Sales Material

The following material is available for the launch:

 

Product Packaging

The Intelli-Arc Diagnostic Tool comes in a plastic carrying case, embossed with the Siemens logo. The case includes the items below.

Click here to view the packaging in detail.  

 
 

Features

  • Improves troubleshooting accuracy

  • Reduce time spent and number of trips to problem site

  • Simplistic setup: wire in, wire out to use

  • Wireless communication- enables “1 person” troubleshooting

  • Can be used to troubleshoot any AFCI circuit

  • LED Indicators: provides status level for current, ground fault, and arc fault

  • Status Indicators: provides confirmation of power and communication connection

Click here for more detailed features.

 
 


All about AFCI