Skip to Content


Content

About the Siemens Van

The Siemens van and trailer is a self contained traveling counter day/ trade show display. The van is available to Siemens Marketing Managers and Sales Engineers to use at customer events.

The van contains eye catching graphics that promote Siemens' products, NASCAR relationship, and marketing programs. It also acts as a storage area for a 10'x10' tent, 6' table, Siemens table cloths, sample product, product display towers, and a propane gas grill.

The trailer also has eye ctaching graphics that promote the Siemens Generator product line. Inside the trailer is a 17 kw standby generator and the new Generator Ready Load Center. Both are operational and are powered by a 120V source and a self contained propane tank.

Van Features

Click images to enlarge

Logistics

Reserving the van
The Regional Marketing Manager (CMM) will make the reservation for the van with product Management - RPDProductManagement.sea@siemens.com

Literature
There is no literature in the van. The local Sales Engineer is responsible for making sure that literature is available at the event.

Transportation
The Sales Engineer or CMM is responsible for transporting the van to and from the event.

Maintenance
The business unit will maintain the van when it is in Atlanta. When on the road, van maintenance, including oil changes, propane tank refilling (trailer and grill), and washing is the responsibility of the local Sales Engineer that is in possession of the van. All such maintenance must be up to date before passing the van onto the next Sales Engineer (if it is not returned to the business unit in between).